SMART MANUFACTURING

Empowering manufacturers with Real-time Machine Health Insights

TDK SensEI: Delivering Edge AI to Enhance Efficiency Across Smart Sectors.

Fantasy image of two workers standing next to machines which have monitoring information floating in front of them.
Fantasy image of digital lines acting as monitoring information floating above machines in a factory.

Smart Manufacturing

In today’s manufacturing environment, unplanned downtime, aging equipment, and limited visibility into machine health remain persistent challenges. Many manufacturers still rely on reactive or schedule-based maintenance, leading to costly failures, inefficient production, and missed performance opportunities. Data overload, siloed systems, and the lack of real-time, actionable insights further complicate efforts to maintain consistent reliability at scale.
 
TDK SensEI’s AI-driven solutions are purpose-built to address these challenges head-on. By leveraging Edge AI, we enable continuous, real-time monitoring of machine health and production performance—directly at the source. Our industrial predictive maintenance capabilities detect subtle anomalies, predict failures before they occur, and eliminate unnecessary maintenance, dramatically reducing downtime and maintenance costs.
 
With deeper visibility into equipment behavior and process variability, manufacturers can move from reactive firefighting to proactive, data-driven decision-making—improving reliability, optimizing throughput, and ensuring consistent product quality across operations.

While manufacturers move toward Industry 4.0, many still face unplanned downtime, reactive maintenance, and limited visibility into machine health. Legacy monitoring systems rely on static thresholds, delayed analysis, and cloud‑dependent workflows that miss early failure signals and create excessive false alarms—slowing digital transformation instead of enabling it.

TDK SensEI’s edgeRX™ puts AI‑driven intelligence directly at the edge. The platform analyzes high‑frequency machine and sensor data in real time, learning normal operating behavior and detecting subtle anomalies before failures occur. By running advanced machine learning models at the source, edgeRX™ eliminates latency, reduces data overload, and delivers reliable insights—even in offline or bandwidth‑constrained environments.

Adaptive to each machine, process, and operating condition, edgeRX™ improves diagnostic accuracy while minimizing false alerts. This enables true predictive maintenance, reduced downtime, and optimized operations at scale. With TDK SensEI, manufacturers don’t just keep pace with change—they anticipate it, unlock new efficiencies, and set new benchmarks for operational excellence.

While manufacturers move toward Industry 4.0, many still face unplanned downtime, reactive maintenance, and limited visibility into machine health. Legacy monitoring systems rely on static thresholds, delayed analysis, and cloud‑dependent workflows that miss early failure signals and create excessive false alarms—slowing digital transformation instead of enabling it.

TDK SensEI’s edgeRX™ puts AI‑driven intelligence directly at the edge. The platform analyzes high‑frequency machine and sensor data in real time, learning normal operating behavior and detecting subtle anomalies before failures occur. By running advanced machine learning models at the source, edgeRX™ eliminates latency, reduces data overload, and delivers reliable insights—even in offline or bandwidth‑constrained environments.

Adaptive to each machine, process, and operating condition, edgeRX™ improves diagnostic accuracy while minimizing false alerts. This enables true predictive maintenance, reduced downtime, and optimized operations at scale. With TDK SensEI, manufacturers don’t just keep pace with change—they anticipate it, unlock new efficiencies, and set new benchmarks for operational excellence.

Beyond software

Monitoring Solutions to Promote Efficiency and Reduce Machine Downtime.

Icon representing monitoring using a heart and heartbeat.

Real-Time Visibility into Critical Production Assets

Manufacturing operations rely on complex, high‑value equipment such as motors, gearboxes, conveyors, robotics, and production machinery. edgeRX™ delivers real‑time insight directly at the machine level, giving plant and maintenance teams continuous visibility into asset health without waiting on centralized analysis. This immediate awareness enables faster response, reduced uncertainty, and better control over production performance.

Depiction of multiple devices showing TDK SensEI's edgeRX™ platform.
Icon representing edge computing.

Proactive Maintenance Without Production Interruptions

Rather than reacting to failures after they disrupt output, edgeRX™ enables proactive maintenance by identifying developing issues early and locally. By processing data at the edge, maintenance teams can address problems during planned windows—reducing unexpected downtime, avoiding line stoppages, and keeping production schedules on track.

Image of TDK SensEI's edgeRX™ LYNQ sensor.
Icon representing scalable factory growth with a gear and bar graph.

Scalable, Always-On Intelligence Across the Factory Floor

Manufacturing environments often span multiple lines, cells, and facilities. edgeRX™ provides a scalable foundation for machine intelligence by running analytics where equipment operates—minimizing network dependency and simplifying deployment across the factory floor. This approach supports consistent maintenance strategies while reducing operational complexity and long-term costs as operations scale.

TDK SensEI product edgeRX™ dashboard opened on a laptop, being used by a maintenance worker.
Beyond software

Monitoring Solutions to Promote Efficiency and Reduce Machine Downtime.

Real-Time Visibility into Critical Production Assets

Manufacturing operations rely on complex, high‑value equipment such as motors, gearboxes, conveyors, robotics, and production machinery. edgeRX™ delivers real‑time insight directly at the machine level, giving plant and maintenance teams continuous visibility into asset health without waiting on centralized analysis. This immediate awareness enables faster response, reduced uncertainty, and better control over production performance.

Depiction of multiple devices showing TDK SensEI's edgeRX™ platform.
Image of TDK SensEI's edgeRX™ LYNQ sensor.

Proactive Maintenance Without Production Interruptions

Rather than reacting to failures after they disrupt output, edgeRX™ enables proactive maintenance by identifying developing issues early and locally. By processing data at the edge, maintenance teams can address problems during planned windows—reducing unexpected downtime, avoiding line stoppages, and keeping production schedules on track.

TDK SensEI product edgeRX™ dashboard opened on a laptop, being used by a maintenance worker.

Scalable, Always-On Intelligence Across the Factory Floor

Manufacturing environments often span multiple lines, cells, and facilities. edgeRX™ provides a scalable foundation for machine intelligence by running analytics where equipment operates—minimizing network dependency and simplifying deployment across the factory floor. This approach supports consistent maintenance strategies while reducing operational complexity and long-term costs as operations scale.

Beyond software

Monitoring Solutions to Promote Efficiency and Reduce Machine Downtime.

Depiction of multiple devices showing TDK SensEI's edgeRX™ platform.

Real-Time Visibility into Critical Production Assets

Manufacturing operations rely on complex, high‑value equipment such as motors, gearboxes, conveyors, robotics, and production machinery. edgeRX™ delivers real‑time insight directly at the machine level, giving plant and maintenance teams continuous visibility into asset health without waiting on centralized analysis. This immediate awareness enables faster response, reduced uncertainty, and better control over production performance.

Image of TDK SensEI's edgeRX™ LYNQ sensor.

Proactive Maintenance Without Production Interruptions

Rather than reacting to failures after they disrupt output, edgeRX™ enables proactive maintenance by identifying developing issues early and locally. By processing data at the edge, maintenance teams can address problems during planned windows—reducing unexpected downtime, avoiding line stoppages, and keeping production schedules on track.

TDK SensEI product edgeRX™ dashboard opened on a laptop, being used by a maintenance worker.

Scalable, Always-On Intelligence Across the Factory Floor

Manufacturing environments often span multiple lines, cells, and facilities. edgeRX™ provides a scalable foundation for machine intelligence by running analytics where equipment operates—minimizing network dependency and simplifying deployment across the factory floor. This approach supports consistent maintenance strategies while reducing operational complexity and long-term costs as operations scale.

Got Questions?

edgeRX™’s edge AI can identify additional fault states outside of conventional ISO frameworks, providing users with deeper insights into the condition of their machines. This advanced capability allows for comprehensive monitoring and proactive maintenance, ensuring optimal machine performance.

edgeRX™ can monitor a wide range of equipment, including rotating machinery, pumps, motors, gearboxes, conveyors, and other critical production assets. The platform adapts to different machines, processes, and production workloads.

YesedgeRX™ is designed to scale from individual machines to entire production lines and multi‑site enterprises. The platform supports consistent deployment and insights across facilities while adapting to local operating conditions.

Traditional alarms trigger when a fixed limit is crossed, often generating noise during normal operation. edgeRX™ uses adaptive AI models that understand what’s normal for each machine and process, alerting only when behavior truly deviates from expected performance.

AbsolutelyedgeRX™ performs analytics directly at the machine level, allowing plants to operate without constant cloud connectivity and avoid sending large volumes of raw sensor data across the network.

YesedgeRX™ can be deployed on a single critical asset, across a line, or scaled plant‑wide, making it suitable for targeted reliability projects as well as broader smart manufacturing initiatives.

Picture of two workers attending to a machine.

Let’s have a conversation about Downtime, Blind Spots, and Reactive Maintenance. ​​We’ll keep you up and running.