Article Link: https://www.automation.com/en-us/articles/august-2025/solving-industrial-machine-health-challenges-edge
In modern manufacturing environments, downtime is a relentless disruptor. When machines fail unexpectedly, operations grind to a halt, triggering cascading delays across production lines, missed delivery schedules and costly labor reallocations. Maintenance teams scramble to identify faults and source replacement parts.
Equipment that fails prematurely not only interrupts the production workflow but also undermines confidence in quality and reliability. For manufacturers already managing tight margins and lean operations, even a brief interruption can create lasting consequences.
For decades, scheduled maintenance has served as the industry’s frontline defense against this risk. However, rigid service intervals often result in servicing equipment too early or too late. In many cases, ISO-based condition monitoring strategies are used to track vibration and performance thresholds. While this method offers a more data-informed approach, it can still fall short. These systems often miss nuanced fault patterns and rely heavily on predefined parameters that don’t account for machine-specific behaviors or variations in load and usage.
From ISO to Intelligence
A growing number of manufacturers are now turning to predictive maintenance (PdM) technologies to overcome these limitations. Unlike condition-based monitoring (CbM), which reacts to predefined fault signals, predictive systems recognize the precursive indicators of failure, allowing timely and accurate servicing. AI-driven solutions deployed directly on the edge are making this possible, enabling real-time monitoring and decision-making where the data originates: on the factory floor. Minimizing latency and reducing reliance on cloud connectivity, edge AI enables faster insight with improved data privacy, reliability and responsiveness.
Edge AI in action
Traditional monitoring solutions rely on transmitting large volumes of raw data to the cloud for analysis and processing. This method not only consumes bandwidth and drains power but also creates delays in detection and response. In some cases, data is collected manually at specific time intervals, with significant time gaps in data collection. Edge AI solves these issues by embedding AI directly onto the sensor itself. Machine learning models trained on past machine behavior can operate locally, detecting anomalies in vibration, temperature, or motion patterns without requiring constant cloud communication. This localized inference significantly enhances the responsiveness of predictive systems while extending battery life and conserving network resources.
A key advantage of edge AI-based systems is their ability to learn and adapt over time. When a machine exhibits a subtle change in behavior that precedes a breakdown, such as an unusual frequency of vibration, AI algorithms can recognize that pattern. If a similar issue occurs again, the system will recognize the signature.
The ability to improve differentiation between benign anomalies and true failure precursors helps reduce the number of false positives. It also allows for more precise fault localization, guiding technicians to the likely point of failure rather than issuing broad warnings.
What future-proof PdM requires
A future-proof predictive maintenance solution must offer more than just technical sophistication. It must be simple to deploy, intuitive to use, and flexible enough to evolve with dynamic operations. Plug-and-play deployment without complex integration is essential for busy facilities with limited IT resources. The most effective systems provide built-in anomaly detection that considers not just the presence of a fault, but also its severity, frequency, and location. Sensitivity controls allow operations teams to tailor alert thresholds to the specific needs of their environment, whether they’re managing high-risk infrastructure or relatively low-impact machinery.
Scalability is another critical factor. In dynamic industrial settings, the ability to move sensors from one machine to another, or to apply a proven model to a different facility, is vital. A good predictive maintenance platform must be able to work across various equipment types and environments without requiring constant recalibration or different system specifications. Systems that are agnostic to the type of machinery they monitor deliver greater value and adaptability over time.
Across industries and infrastructure
These capabilities are being applied across a wide array of industries. In smart manufacturing, predictive systems monitor everything from conveyors and cutting machines to robotic arms. Pumps and motors are constant targets for failure detection given their tendency and sensitivity to wear. In building systems, predictive maintenance can improve the reliability of HVAC infrastructure and elevators. Energy applications include the monitoring of turbines, battery systems and transformers, where performance drift can lead to both efficiency losses and safety risks. The diversity of use cases highlights the need for a flexible, hardware-agnostic platform that can support virtually any environment.
The edgeRX Model
The edgeRX platform is one example of what this next generation of machine health monitoring can look like. Developed by TDK SensEI, edgeRX combines an industrial grade sensor node, gateway, reporting dashboard and cloud interface into a unified, out-of-the-box solution. Once deployed, the system automatically begins collecting data and classifying operational states, eliminating the need for manual input or data labeling.
Once a machine learning model is constructed, it can be pushed to the sensors to begin analyzing data in real time, flag anomalies and learn from behavior patterns over time.
Because edgeRX runs its models on-device, it avoids the energy costs and latency associated with cloud-based inference. This also enhances data security, as inference occurs on the sensor rather than in the cloud.
The hardware is built for industrial use, featuring IP67-rated enclosures, long-life batteries, and compatibility with harsh temperature environments. With minimal user involvement, edgeRX delivers rapid insights and fast time-to-value, making it excellent for large-scale deployments or facilities with limited engineering resources.
Delivering on Industry 4.0
As organizations continue to evaluate their machine health monitoring practices, they should consider the following: Importance of fault detection, accuracy of current detection methods, and current ability to scale.
Edge-AI-enabled predictive maintenance will move manufacturers toward smarter, more autonomous operations. Predictive systems like edgeRX are a natural fit for Industry 4.0 strategies. They empower teams to make more informed maintenance decisions with less effort, extend the lifespan of critical assets, and respond to emerging issues before they become disruptive failures. The shift from reactive to proactive maintenance is well underway, and edge-based AI is accelerating that transformation.
As manufacturers embrace smarter, more autonomous operations, edge AI platforms like edgeRX are becoming vital to Industry 4.0 strategies, enabling faster, more informed maintenance decisions, extending asset life and preventing failures before they disrupt production. The shift from reactive to proactive maintenance is accelerating, and organizations must ask: Are our systems keeping up? If they can’t detect early faults, scale easily, or deliver real-time insights, it may be time to rethink what effective predictive maintenance really looks like.